Hello,
We use
- S32K144W
- S32DS 3.3
- SDK RTM 4.0.1
- CAN without FD
Maybe this is something wrong, but in which context CANx_Error_IRQHandler is called?
Is there any example for handling CAN bus errors using the FlexCan driver?
Basically, we disconnect the CAN bus which means an aknowledge error, but it is never called. We have introduced error in the bus and this fuctions is never called
We saw that in FLEXCAN_EnableIRQs::L617 the IRQ is enabled. However, we are not sure in which context CANx_Error_IRQHandler is called
Thanks in advance,
Solved! Go to Solution.
Hi,
I tested error interrupt/callback using below example, I posted. It is using older SDK, but it should be similar, I guess.
BR, Petr
Thanks PetrS
Hi,
I tested error interrupt/callback using below example, I posted. It is using older SDK, but it should be similar, I guess.
BR, Petr