Erase FLASH,S32K144 Reset,why?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Erase FLASH,S32K144 Reset,why?

9,901件の閲覧回数
eautopower
Contributor IV

hello

boot memory configure:

pastedImage_1.png

APP memory configure:

pastedImage_2.png

erase code:

pastedImage_3.png

if code run here,the S32K144 reset:

pastedImage_4.png

pastedImage_5.png

9 返答(返信)

7,501件の閲覧回数
jinshuaixu
Contributor V

Hi,friend

     Did you have close interrupt? if you operate FLASH, you must close interrupt .

/* Erase the two PFlash sector */
address =ccp_save_address;
size = FEATURE_FLS_PF_BLOCK_SECTOR_SIZE*2;
ret = FLASH_DRV_EraseSector(&flashSSDConfig, address, size);
EnableInterrupts
if (ret != STATUS_SUCCESS)
{
while(1);
}

7,502件の閲覧回数
tuozhou
Contributor II

hi,

   I'm having a similar problem,when I use the EEE partition,I jump to the Reset_Handler ,and I disable interrupt by use "cpsid i".

0 件の賞賛
返信

7,502件の閲覧回数
tuozhou
Contributor II

I see the RCM->SRS and I found Core lock up occurs when jump to the Reset_Handler.

7,502件の閲覧回数
eautopower
Contributor IV

Hi jinshuai:

 yes,you are right,thank you!

another problem:

do you know the jump to APP code ?I don't how to jump,if you know send me mail: [email protected] ,thank you very much!

0 件の賞賛
返信

7,502件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

take a look at:

https://community.nxp.com/message/907130 

Regards,

Lukas

0 件の賞賛
返信

7,502件の閲覧回数
eautopower
Contributor IV

hi:

like this?

pastedImage_1.png

0 件の賞賛
返信

7,502件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

If 0x8004 is address of reset vector then yes.

Regards,

Lukas

0 件の賞賛
返信

7,502件の閲覧回数
eautopower
Contributor IV

hi:

pastedImage_1.png

pastedImage_2.png

is right?

0 件の賞賛
返信

7,501件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

have you disabled interrupts before jumping to user app? It is also good idea to reconfigure the device to default reset state. Or the user app must be aware that not everything is in default reset state.

If you step the asm code, are you able to get to start up code of user app? Where does it crash?

Regards,

Lukas

0 件の賞賛
返信