EB Tresos warning for ADC module of S32K1XX

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

EB Tresos warning for ADC module of S32K1XX

1,281件の閲覧回数
shudhamatinarha
Contributor II

Hello, 

getting following warning when I reopen my ADC configuration in EB Tresos.

Configurations has no error or warnings related to ADC this warning is only popping up while opening the project and its not affecting validation or generation but want to know what warning means exactly,.

"Node /TS_T40D2M10I1R0/Adc/AdcConfigSet/AdcHwUnit/AdcGroup/AdcEnableHalfInterrupt defines two attributes with the same name "EDITABLE" which could not be merged. Removing one of the attributes"

Note: I haven't configured anything related to half interrupt.

Thank you in advance. 

0 件の賞賛
返信
1 返信

1,268件の閲覧回数
hungnguyenphi
NXP Employee
NXP Employee

Dear Shudhamatinarha,

This is an error in the MCAL package. This issue has been fixed in the S32K14X_MCAL4_2_RTM_1_0_4 package.

Best regards,

Hung.