I am trying to capture the Cam and Crank signals with input Edge Capture block i am using module 0 for both signals but each as separate pins the crank has 34 teeth and 2 missing teeth for 1 revolution the block parameters that i am using is prescale factor of 1 and ISR priority 5 the input frequency is 500Hz and the freemaster value are not making any sense . If any one can help me with that .
Can you provide a detailed description of the problem?
Including the MCU configuration, the input signal paremeters, etc.
Thank you,
BR, Daniel
S32k144-EVB