Comparator of S32k146

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Comparator of S32k146

439 Views
Shruthi_C
Contributor II

HI,

I want to configure comparator-0 with IN6 and IN7 as comparator inputs 

and also IN6 should be fixed input pin to comparator with 1V

IN7 is varying input to comparator,

My requirement is when IN7 is less that IN6 voltage (1V) I have to get comparator output,

Please can I get configuration and code support on this?

0 Kudos
Reply
2 Replies

278 Views
Shruthi_C
Contributor II

HI Robin

Thanks

0 Kudos
Reply

417 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Please refer to Example S32K144 CMP Windowed Mode use PDB S32DS3.4 RTM4.0.3

Hope it helps.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply