ADC is always BUSY and Conversion does not complete
when i add a while loop to check the ADC mode is BUSY the control stays in this while loop
I am trying to Read the Pin values using Adc_Readgroup
but to read successfully the conversion should be complete
I am calling functions
Adc_Calibrate(AdcGroup_0,&adc0_cal_status);
/* Setup the variables to contain the ADC results */
Adc_SetupResultBuffer(AdcGroup_0, &ADC_Group0Results[0]);
/* Initiate the initial conversion */
Adc_StartGroupConversion(AdcGroup_0);
before calling
Adc_ReadGroup(AdcGroup_0,&ADC_Group0Results[0]);
kindly find the configuration file below
解決済! 解決策の投稿を見る。
Hi man,
Did you enable the Port Pin for ADC, and the Clock in MCU? Just hint for you.
Hi Vinhnguyen
The problem is resolved the problem was I have two versions of the project there is no issue in the older version. When you replied i did checked the port pins and Mcu clock. the port pin was enabled and Mcu clock was set to SIRC. At later point of time when i was comparing the two versions i found that SIRC was not under Mcu control so i changed to SOSC clock now it works
Your hint helped though but i was late to find it
Hi VinhNguyen
Thank You for the reply
Port pins are enabled in PORT and Clock(4Mhz SIRC) is enabled for ADC in MCU
Regards
Akbar