ADC SW triggered while ADC triggered by BCTU

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ADC SW triggered while ADC triggered by BCTU

1,332 次查看
Simone9
Contributor III

Hello,

I am working on a motor control project with the S32K324 micro based on the MCTPTX1AK324 demoboard example.
I have implemented the mechanism of perdiodic acquisition from the three ADCs via the EMIOS -> BCTU -> ADC chain with a frequency of 20KHz in interrupt, of which there are two sequences, managed by two different channels of the EMIOS0 (every 25us starts a new acquisition of new BCTU List).

I wanted to manage not only these scheduled acquisitions but also acquisitions to be started via SW, to be managed with periodic starts and without DMA with lower acquisition time.
So, I wanted to ask if it was possible and how to do it without interfering with the interrupt acquisitions?
There is some exampe that handle this situation?

 

Thank you very much.

 

IDE S32 Design Studio 3.5
RTD 3.0.0

0 项奖励
回复
3 回复数

1,311 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@Simone9

In this demo (MCSPTE1AK344), there is a program that uses software to trigger the ADC to sample the temperature sensor, which should be the same as your needs.

Senlent_0-1702954849067.png

 

0 项奖励
回复

1,301 次查看
Simone9
Contributor III

Hi,

I have seen these example but the API that you highlight is a specific API releated to the Temperature Sensor not for a generic ADC channel.

What I need is to understand how to set up the RTD driver and the API to call to schedule multiple SW triggered acquisitions, which do not interfere with BCTU acquisitions made via interrupt.

 

Thanks

0 项奖励
回复

1,273 次查看
Senlent
NXP TechSupport
NXP TechSupport

Hi@Simone9

There are two ways for S32K3 software to trigger the ADC.
1.CPU->ADC
2.CPU->BCTU->ADC

In the RTD driver, we have provided ADC sampling example demos for these two methods.

You can refer to these two demos.

Senlent_0-1703126873471.png

 

0 项奖励
回复