32k116 evb unable to debug, and run programs on s32ds

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

32k116 evb unable to debug, and run programs on s32ds

343件の閲覧回数
reidefe
Contributor I

I have the s32k eval board, which is connected through a mini USB  and it is not being recognized by freemaster, also debug doesn't work on s32ds for ARM. On device manager in windows, the device is recognized via the opensda COM port, and also the same ins32ds debugger but for some reason, it can't connect to it, same as on freemaster. 
I have copied the S32K116_EVB_JumpStart_Firmware.srec into the device folder, and it blinks 8 times and 2-sec timeout. I have tried using a 12v external power source, but still no success. I managed to get into the bootloader mode, but even then it can't do anything.

0 件の賞賛
返信
1 返信

299件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 

Please refer to the discussion in S32K116EVB FreeMaster Connection Failure


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信