使用底层代码会导致不符合autosar规范吗?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

使用底层代码会导致不符合autosar规范吗?

601 Views
sophie-wang
Contributor III

Hi NXP,

想请教一下,如果我需要使用的功能上层函数不能实现,需要调用底层接口函数,会导致不符合autosar规范吗?

感谢

Sophie

0 Kudos
Reply
1 Reply

588 Views
StephenDu
NXP Employee
NXP Employee

Hi, Sophie

In order for others to view this topic as well, I'll translate your question in English.

Question: Will using the underlying code result in non-compliance with the AUTOSAR specification?

Answer: AUTOSAR standard itself does not prohibit access to the underlying interface (although the standard modules are specified in very detail API information, but it can also be extended according to the actual usage). But usually, the underlying API is not exposed to the public, and the API style is different, from this point of view, it is not meet the standard(The extension introduced above, commonly means extend the API at the same layer). I suggest you bring up the specific requirements and let the development team see if they can provide a new interface for access at the upper layer to meet your needs.

0 Kudos
Reply