Hi, NXP
I am using BSP33.0 on s32g274ardb2.
1. When I run the "reboot" command on the linux with core A, the M7 core will also restart.
Is there any configuration that can restart the A core independently without affecting the M7 core ?
2. When the M core crash abnormally, it will also cause the A core to break down,
and the system log of the A core can not record the reason for the forced restart.
Is there a method to record logs of above scene ?
Thank you for your reply.
After our verification, the command "halt" can shut down core A alone, while core M does not shut down or restart, command "halt --reboot" restarts both core A and core M. We want to find the way to restart kernel A alone.
Hi @eone,
Resetting the A53 core without impacting the M7 core is possible but there are no commands available for that. You need to read the reference Manual A53 Reset Sequence and develop code for the same.
A53 core is running Linux OS and suggested not resetting it as it can corrupt the OS Functionalities.
Thanks,
Mayank S Patel
Hi @eone,
Thank you for reaching out to us.
Please find the answer below:
1. you can use the "halt" command for independently resetting the A53 core. This will not reset the M7 core.
2. Please follow the steps for preserving system logs.
Hope this helps.
Thanks,
Mayank S Patel