about add M.2 SSD disk for S32G ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

about add M.2 SSD disk for S32G ?

348件の閲覧回数
hardy2023
Contributor I

hi, experts,

I am working with  S32G  with a ubuntu 18.04 used SD card as boot device,

and I found the read write speed is realy slow , I use some tool have a test.

with 1G file random IO test .

Read 14.7 M/S
Write 3.42 M/S
 
it's slow to run my docker system.
So I want add a M.2 SSD disk for S32G. 
for the board has a M.2 E-key Slot (J47) and M.2 M-key Slot  (J56) ,maybe can insert a SSD?
did any one know which SSD can work with this slot, or any suggestion about speed up IO?
 
ラベル(1)
タグ(1)
0 件の賞賛
返信
0 返答(返信)