Why failed to boot flash bootloader by bsp35.0 u-boot-s32g399ardb3.bin-qspi ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Why failed to boot flash bootloader by bsp35.0 u-boot-s32g399ardb3.bin-qspi ?

Jump to solution
1,104 Views
fengxianeric
Contributor IV

I used ds flashtool to program flash with this image, why failed to boot ? 

but when I burned fsl-image-flash-s32g399ardb3.flashimage, it can boot whole system.

what is the reason for this scenario ? thanks

0 Kudos
Reply
1 Solution
1,032 Views
nxf92355
NXP Employee
NXP Employee

Hi Eric Li

Q. The image fip.s32-qspi under my compiled directory of s32g399ardb3/ from bsp 35.0,  so can I program this image directly to flash 0x0 place ? 

=> Yes , you can directly flash using S32Flashtool ,from 0x0

Q.  BTW, I see related 2 tools here, what does it do for ?

=> qspi_params_MX25UW51245G.bin is for MX25UW51245G NOR Flash memory and

     u-boot-s32.cfgout-qspi contains location of configuration files

 

please use flashtool @ /NXP/S32DS.3.5/S32DS/tools/S32FlashTool/GUI/  to flash image.

read user guide @/NXP/S32DS.3.5/S32DS/tools/S32FlashTool/doc/S32_Flash_Tool_User_Guide.pdf

 

Regards ,

Tushar

View solution in original post

0 Kudos
Reply
3 Replies
1,048 Views
nxf92355
NXP Employee
NXP Employee

Hi Eric Li

Hope you are doing well.

The image u-boot-s32g399ardb3.bin-qspi does not contain dtb and IVT. so board will not boot using that image. Now TF-A (Arm Trusted firmware) is a mandatory component of the boot.So use the image fip.s32-qspi to boot. you will find this image in arm-trusted-firmware. let us know if any quarry.

 

Regards ,

Tushar

 

0 Kudos
Reply
1,041 Views
fengxianeric
Contributor IV

Thanks.

The image fip.s32-qspi under my compiled directory of s32g399ardb3/ from bsp 35.0,  so can I program this image directly to flash 0x0 place ? 

---------------------------------------------------------

BTW, I see related 2 tools here, what does it do for ?  thanks.

eric@eric-VirtualBox:~/myspace/nxp/s32g3/arm-trusted-firmware$ ls -l /home/eric/myspace/disk1/backupimgs/myimage/s32g399ardb3/tools/
total 20
-rwxr-xr-x 1 root root 508 4月 20 17:16 qspi_params_MX25UW51245G.bin
-rwxr-xr-x 1 root root 4904 4月 20 17:16 u-boot-s32.cfgout-qspi

0 Kudos
Reply
1,033 Views
nxf92355
NXP Employee
NXP Employee

Hi Eric Li

Q. The image fip.s32-qspi under my compiled directory of s32g399ardb3/ from bsp 35.0,  so can I program this image directly to flash 0x0 place ? 

=> Yes , you can directly flash using S32Flashtool ,from 0x0

Q.  BTW, I see related 2 tools here, what does it do for ?

=> qspi_params_MX25UW51245G.bin is for MX25UW51245G NOR Flash memory and

     u-boot-s32.cfgout-qspi contains location of configuration files

 

please use flashtool @ /NXP/S32DS.3.5/S32DS/tools/S32FlashTool/GUI/  to flash image.

read user guide @/NXP/S32DS.3.5/S32DS/tools/S32FlashTool/doc/S32_Flash_Tool_User_Guide.pdf

 

Regards ,

Tushar

0 Kudos
Reply