What is the Behavior of PMIC using external Watchdog (Wdg_43_VR5510)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the Behavior of PMIC using external Watchdog (Wdg_43_VR5510)

209 Views
Anup97
Contributor II

I have implemented the external watchdog (Wdg_43_VR5510) for PMIC. But it is going into endless loop in Pmic_VR5XX_TimeoutLoops_StateTransistion (refer below).

Anup97_0-1728381149960.png

Currently it is in INIT_FS state, as per the state diagram it says we need to have a good watchdog refresh to change the state from INIT_FS to Wait_ABIST2.

Anup97_1-1728382345854.png

To Satisfy the first good watchdog refresh within 256ms, we have called watchdog trigger API after Wdg_43_VR5510_Init function during EcuM Initialization.

Anup97_2-1728382440162.jpeg

We need to know, how and where to call the first watchdog refresh. So that the state transition happens from INIT_FS to wait_ABIST2.

Tags (1)
0 Kudos
Reply
2 Replies

161 Views
Anup97
Contributor II

Thank you @Celeste_Liu.

0 Kudos
Reply

172 Views
Celeste_Liu
NXP Employee
NXP Employee

Dear @Anup97 ,

Thanks for contacting us. We are following this same inquiry with another member of your company. We will mirror this issue to another thread (link: Behavior-of-PMIC-using-external-Watchdog-Wdg-43-VR5510 ). Thank you for your understanding and support.

Best Regards,

Celeste

0 Kudos
Reply