S32g FLS The routine is not a complete one to make using EB tools

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32g FLS The routine is not a complete one to make using EB tools

657 Views
jianqun
Contributor II

Fls_TS_T40D11M30I2R0


static void Fls_PinSetup(void)
{
IP_SIUL2_0->MSCR[85] = 0x00280021U; /*QSPI_A[0]*/
IP_SIUL2_0->MSCR[86] = 0x00280021U; /*QSPI_A[1]*/
IP_SIUL2_0->MSCR[87] = 0x00280021U; /*QSPI_A[2]*/
IP_SIUL2_0->MSCR[88] = 0x00280021U; /*QSPI_A[3]*/
IP_SIUL2_0->MSCR[89] = 0x00280021U; /*QSPI_A[4]*/
IP_SIUL2_0->MSCR[90] = 0x00280021U; /*QSPI_A[5]*/
IP_SIUL2_0->MSCR[91] = 0x00280021U; /*QSPI_A[6]*/
IP_SIUL2_0->MSCR[92] = 0x00280021U; /*QSPI_A[7]*/
IP_SIUL2_0->MSCR[93] = 0x00280021U; /*QSPI_A Data strobe*/
IP_SIUL2_0->MSCR[96] = 0x00200021U; /*QSPI_A Serial Clock*/
IP_SIUL2_0->MSCR[97] = 0x00200021U; /*QSPI_A Serial Clock*/
IP_SIUL2_0->MSCR[98] = 0x00200021U; /*QSPI_A Serial Clock*/
IP_SIUL2_0->MSCR[99] = 0x00200021U; /*QSPI_A Serial Clock*/
IP_SIUL2_0->MSCR[100] = 0x00203021U; /*QSPI_A Chip select*/
IP_SIUL2_0->MSCR[101] = 0x00203021U; /*QSPI_A Chip select*/

IP_SIUL2_0->IMCR[28] = 0x00000002;
IP_SIUL2_0->IMCR[29] = 0x00000002;
IP_SIUL2_0->IMCR[30] = 0x00000002;
IP_SIUL2_0->IMCR[31] = 0x00000002;
IP_SIUL2_0->IMCR[32] = 0x00000002;
IP_SIUL2_0->IMCR[33] = 0x00000002;
IP_SIUL2_0->IMCR[34] = 0x00000002;
IP_SIUL2_0->IMCR[35] = 0x00000002;
IP_SIUL2_0->IMCR[36] = 0x00000002;

/*QSPI_A INTERRUPT: ECC error signal, Flash Memory A drives this signal to active low value in case of an ECC error */
IP_SIUL2_0->MSCR[94] = 0x00083020; /* Disable OBE; Enable IBE; Enable pull-up */
IP_SIUL2_0->IMCR[37] = 0x00000002;
}

  • Is there a full standard auotsar routine

 
0 Kudos
Reply
3 Replies

635 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Can you let us know which RTD version are you using? We assume RTD v3.0.2, but we would like confirmation.

Please, let us know.

0 Kudos
Reply

618 Views
jianqun
Contributor II

yes,SW32G_RTD_4.4_3.0.2_HF01_D2204 is This RTD is the version, but I can't find a matching package for HSE BOOTLOAD

0 Kudos
Reply

594 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Thanks for your feedback. It seems your last comment might be referring to the following thread:

Re: SW32G_RTD_4.4_3.0.2_HF01_D2204,Is there any pa... - NXP Community

If so, information has been provided in there. As for Fls example with full autosar routine, it seems that this might be fulfilled by using RTD v4.0.0, since we see that there is no "Fls_PinSetup(void)" function usage and it is replaced by "Port_Init(NULL_PTR)".

Please, let us know.

0 Kudos
Reply