S32G Reference Design Board 2 - compilation and wifi

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32G Reference Design Board 2 - compilation and wifi

1,765 Views
manra
Contributor I

Please, I need to enable a wifi card on S32G Reference Design Board 2 using the linux distro.

Can someone send me instructions how to compile and tell me if the configuration must be similar to have wifi on imx6 ?

Any info is very welcome and very appreciated. 

0 Kudos
Reply
1 Reply

1,739 Views
bpe
NXP Employee
NXP Employee

Instructions on enabling externally connectable peripherals and building the
corresponding software are typically provided by the peripheral manufacturer.
Since it is about Linux, the steps should in general be the same for any
platform, however, I suggest checking with your WiFi card documentation if
there are any special instructions or known issues with ARM64 targets. If
you are looking for generic instructions on how to (re)configure and build a Linux
kernel for S32G2, refer to Automotive BSP User Guide, Chapter 2. This document
is available through Flexera, together with the rest of the BSP files, under
S32G2 Reference Software. Note that NXP provide different Linux BSPs for i.MX
and S32G families.

Best Regards,
Platon

0 Kudos
Reply