S32G LLCE-1.0.4 version CAN2CAN project : does not match target or release version

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32G LLCE-1.0.4 version CAN2CAN project : does not match target or release version

1,201 Views
Jitender1203
Contributor III

Hi,

Very strange error. Goldvip 1.5.0 CAN-gw Eb tresos project target is different with S32G2-LLCE-1.0.4 Eb tresos project target name is different. How to fix this issue?? 

LLCE-1.0.4 plugins loading into EBtresos -- LLCE plugins itself getting error does not match target or release version.  unable to get those target matched plugins and with version plugins.

Jitender1203_0-1680701955078.png

 

Please help in plugins issue to fix, so that we can progress to configure.

Regards,

Jithu

 

0 Kudos
Reply
4 Replies

1,120 Views
viswa_kondapall
Contributor IV

Hi Daniel,

Sorry to jump into this thread. To avoid duplicate, so posting. PFE loaded good to me(RTD3.0.2: 8-10 plugs , LLCE 1.0.4: 3 plugins, PFE-mcal 0.9.7 - ETH-43 only one plugin ). These only copied and PFE is loaded perfect once copied plugins. BUT with the same plugins CAN2CAN has issue as below. Shall i post here or to create another thread, below image may helps in understanding the error.

viswa_kondapall_1-1681147020132.png

regards,

Viswa

 

0 Kudos
Reply

1,186 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

We are not seeing the same behavior as the one you have. Below our result:

DanielAguirre_0-1680724238214.png

Have you modified anything on the plugins folder? We have noticed that once we add more plugins into Tresos, some projects start to fail.

We can recommend starting from a fresh Tresos installation and adding only the required modules.

Please, let us know.

0 Kudos
Reply

1,147 Views
Jitender1203
Contributor III
Hi Daniel,
we didn't modified on the plugins folder. And we already tried with the fresh installation.
0 Kudos
Reply

1,128 Views
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Thanks for your feedback.

When trying a fresh installation, did you only put the needed plugins on the "plugins" folder? Or you used the same "plugins" folder from before?

Since you say that you used GoldVIP example, there were some modifications that were needed for the project. This could be the problem you are seeing.

We can recommend just using the required plugins from a fresh installation on Tresos. This means:

  • Creating a copy of the "plugins" folder, in case it is needed, then deleting the "plugins" folder (the copy will be the backup).
  • When instaling Tresos, it will automatically create the "plugins" folder if it is not found and add the Tresos required packages.
  • Then you should be able to add the needed plugins for the project (RTD v3.0.2 HF01 + LLCEv1.0.4). 

Please, let us know.

0 Kudos
Reply