Maximum sustained force for heat sink attachment

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Maximum sustained force for heat sink attachment

Jump to solution
1,435 Views
Cooper8121
Contributor I

Hi all,

What's definition of maximum force in Table 5. Maximum force for common Freescale packages.

https://www.nxp.com/docs/en/application-note/AN4871.pdf

Is it sustained force?

Thanks.

Cooper.

 

0 Kudos
Reply
1 Solution
1,427 Views
andrei_skok
NXP Employee
NXP Employee

Yes, this is the maximum sustained force that can be continuously applied to the top of the package.

View solution in original post

0 Kudos
Reply
1 Reply
1,428 Views
andrei_skok
NXP Employee
NXP Employee

Yes, this is the maximum sustained force that can be continuously applied to the top of the package.

0 Kudos
Reply