LLCE issue with S32G

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LLCE issue with S32G

2,693 Views
Paola
Contributor I

Hi,

 

I try to do the example in pag 38 of the guide TP-CONNECTS2021-AUT430.pdf

I use:

  • S32G2XX_LLCE_1.0.1_1.0.1
  • SW32G2_RTD_4.4_2.0.0_P03

Because I don’t download any other .exe in NXP site.

To install these I used:

  • SW32G2_RTD_4.4_2.0.0_P03_D2109.exe
  • S32G2XX_LLCE_GATEWAY_1.0.1_HF1_D2106.exe

I install Tresos ACP-8.8.3_S32G27X downloaded by NXP site

In the folder EB/tresos/plugins I don’t have Bootloader_TS_T40D11M217I0R0. Why?

I try to copy from S32G2XX_LLCE_1.0.1_1.0.1 and SW32G2_RTD_4.4_2.0.0_P03 the folders in tresos/plugins

I open EB tresos 28.1.0 tool and I follow the guide (pag 39).

When I click in test_llce -> Load Configuration I don’t see:

  • CAN_43_LLCE
  • Llce_Af
  • Mcu
  • Port

Why I don’t find them if I added the folders?

For these reasons I don’t able to build the project.

Anyone can tell me where is the problem?

thanks

Paola_0-1658322070107.png

 

0 Kudos
Reply
5 Replies

1,698 Views
ofer-bahar-guardknox
Contributor IV

I also have this LLCE plugin license error within the EB Tresos 

If someone solved this please advise 

Thanks

0 Kudos
Reply

2,209 Views
viswa_kondapall
Contributor IV

Me too facing Plugins issue: We are using Sample CAN2CAN application LLCE 1.5.0 which is latest and respectively EB tresos given few errors so finally find matching Plugins which are latest PFE-1.0.0 and RTD 4.4.4 also. As per the AN13423 we followed, replaced plugins till here all are fine. 

Very strangely after importing while Load Configurations throwing error: target Mismatch or Version mismatch. MCU is correct and respective processor branch only downloaded.  Why this issue is occurring ?? Why NXP is leaving in open issue. No support we are getting in intime.

0 Kudos
Reply

2,651 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello Paola,

 

You must attached the TP-CONNECTS2021-AUT430.pdf I could'nt find it. But surely its Old, The File that you mention its the only you have by installed SW32G2_RTD_4.4_2.0.0_P03_D2109 and S32G2XX_LLCE_GATEWAY_1.0.1_HF1.  The presenter of the file you mentioned use the complete file with tresos, that you can download it from:

https://www.nxp.com/app-autopackagemgr/software-package-manager:AUTO-SW-PACKAGE-MANAGER

 

Regards

 

0 Kudos
Reply

2,647 Views
Paola
Contributor I

Hi,

 

thanks for your feedback.

Attached you can find the file that I used (see pag 42).

I installed Tresos 28.1.0 but I don't have all plugin to do this project. How it is possible?

0 Kudos
Reply

2,307 Views
suresh1
Contributor I

Hi

 

I am also facing the same problem have you resolved it.

If resolved this one, please help me.

I installed same version Tresos 28.1.0.

 

Regards,

Suresh

0 Kudos
Reply