How does it influence the A-Core and M-Core job with the option "m7boot" ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How does it influence the A-Core and M-Core job with the option "m7boot" ?

925件の閲覧回数
fengxianeric
Contributor IV

From the technical chapter within S32G3_LinuxBSP_35.0_User_Manual doc, I got below guidance information,

DISTRO_FEATURES_append += "m7boot"

this document instruct how to build linux fsl packages, but why it refered this information, how does it influence boot M7 core correctly (or building how many files related to M7 core) to run A53 kernel and driver modules smoothingly? 

0 件の賞賛
返信
4 返答(返信)

900件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信

889件の閲覧回数
fengxianeric
Contributor IV

root@s32g399ardb3:~/release0511/poll# ./ipc-shm-sample.elf

Input number of messages to send: 5
ipc-shm-us-app: ch 0 >> 19 bytes: SENDING MESSAGES: 5
ipc-shm-us-app: send_data_msg(): failed to get buffer for channel ID 1 and size 32
ipc-shm-us-app: exit
0 件の賞賛
返信

890件の閲覧回数
fengxianeric
Contributor IV

[ 6.565206] 8021q: adding VLAN 0 to HW filter on device eth0
[ 9.642413] s32cc-dwmac 4033c000.ethernet: Set TX clock to 125M
[ 9.642449] s32cc-dwmac 4033c000.ethernet eth0: Link is Up - 1Gbps/Full - flow control rx/tx
[ 9.642481] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
[ 24.022589] ipc_shm_dev: loading out-of-tree module taints kernel.
[ 85.245931] ipc-shm-sample: starting demo...
[ 85.245948] ipc-shm-sample: ch 0 >> 20 bytes: SENDING MESSAGES: 10
[ 85.245958] ipc-shm-sample: send_data_msg(): failed to get buffer for channel ID 1 and size 32
root@s32g399ardb3:~/release0511#
0 件の賞賛
返信

893件の閲覧回数
fengxianeric
Contributor IV
Yes, thanks, I can understand what it means by mannually invoke m7 work, but about production environment I can't input command by uboot. On the other side my question is about the option which I need to build on linux dev environment. what can it produce after enabled the m7boot option ?
0 件の賞賛
返信