Creating M7 firmware image with IVT for S32G2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Creating M7 firmware image with IVT for S32G2

1,706 Views
yellapu_anishkh
Contributor IV

I am using BSP28, which compiles linux and u-boot.

u-boot with IVT is created, similarly M7 binary with IVT has to be created.

Please point me with the process to compile M7 binary and create IVT for M7 binary

0 Kudos
Reply
1 Reply

1,683 Views
bpe
NXP Employee
NXP Employee

You need S32 Development Studio with support to S32G2 processors installed to
generate IVT for M7 cores. Automotive BSP cannot do it, it has no support to M7 cores.
Familiarize yourself with the document at this link, slides 3 through 24 to see how to
create a bootable image for M7 core. That includes IVT generation.

Hope this helps,
Platon

 

 

0 Kudos
Reply