Couldnt insert one of the kernel modules in IPCF address already in use error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Couldnt insert one of the kernel modules in IPCF address already in use error

554 次查看
ashwini2024
Contributor II

S32G3

BSP 40.0

IPCF 4.10

On m core side: AUTOSAR

On a core :Linux

0 项奖励
回复
3 回复数

539 次查看
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Can you help us elaborate more on regards of the setup you are doing? Which commands are you inputting under uboot? Can you help us sharing the whole boot log of your system?

Is the BSP being built manually with yocto? Or are you using the pre-built images provided by NXP?

Please, let us know.

0 项奖励
回复

472 次查看
ashwini2024
Contributor II

The below is the boot loG. WE are manually building and not pre built images.

0 项奖励
回复

461 次查看
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

Thanks for your feedback. We can recommend using the pre-built images by NXP to isolate any compilation/configuration errors under your custom build. The following community post provides information on regards of manually building the IPCF module and loading into a pre-built image by NXP:

Re: Issue with NXP S32G274A RDB2 -  IPCF - NXP Community

Please, let us know.

0 项奖励
回复