Anyone could tell me the official link to download nxp arm32 bare mental toolchain for M7/S32G?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Anyone could tell me the official link to download nxp arm32 bare mental toolchain for M7/S32G?

1,249 Views
Lake_Hu
Contributor I

Anyone could tell me the official link to download nxp arm32 bare mental toolchain for M7/S32G?

I need this new version.  Thanks 

GNU Bare-Metal Targeted Tools for Arm 32-bit
Embedded Processors
NXP GCC for Arm Release 15-May-2020

0 Kudos
Reply
2 Replies

1,170 Views
asap
NXP Employee
NXP Employee

Lake_Hu, if you are looking for any of below version, it is within the S32DS 3.4 package:

asap_0-1654496760062.png

which can be found on the Automotive Software Package Manager,  S32G2 - Software Library - Tools - S32 Design Studio and Configuration tools.

 

Albert
0 Kudos
Reply

1,190 Views
zhouwg
Contributor II

The ARM toolchain includes the GNU Compiler (GCC) and is available free of charge directly for Windows and Linux  host operating systems. Follow the links on this page to download the correct version for your development environment:

 

Downloads | GNU-A Downloads – Arm Developer

 

Hope it's helpful for you.

0 Kudos
Reply