error in package installation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

error in package installation

2,357件の閲覧回数
hamid_abrishami
Contributor III

Hi every one!
I can't to install online package to I try to do in in a offline way. but it also has error 

"An error occurred while collecting items to be installed
session context was:(profile=DefaultProfile, phase=org.eclipse.equinox.internal.p2.engine.phases.Collect, operand=null --> [R]com.nxp.s32ds.cross.sdk.KEAx_AMMCLIB_1.1.14_root 1.0.0.201811261156, action=).
The required Touchpoint: com.freescale.updater.touchpoint 1.0.0 touchpoint for the collect action is not included in the installation manager configuration.
The required Touchpoint: com.freescale.updater.touchpoint 1.0.0 touchpoint for the collect action is not included in the installation manager configuration."





0 件の賞賛
返信
1 返信

2,342件の閲覧回数
VaneB
NXP TechSupport
NXP TechSupport

Hi @hamid_abrishami 

This issue most cases is caused due to package compatibility problems. Make sure the package is supported by the IDE version. 

 

B.R.

VaneB

0 件の賞賛
返信