CAN transmission works well at SDK02 but does not work at SDK03

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CAN transmission works well at SDK02 but does not work at SDK03

1,829 次查看
kimjunghyun
Contributor III

Hi.

Recently I made CAN message transmission code and it worked well. I confirmed it on the CANoe

* I had some problems so I asked here and PetrS helped me so I could handle it.

  The problem was clock.

 

But after I updated S32DS, this code did not transmit CAN message.

* Of course I changed all components which I used from SDK02 to SDK03.

So I made another new project and I used same code. But CAN transmission did not work.

* Digital input and output worked well.

* CAN related functions executed during debuging (I checked it)

 

Why this code do not transmit CAN message?

 

MCU : S32K144_64pin

TX : PTC7(51pin)

 

<Code>

/* Including needed modules to compile this module/procedure */
#include "Cpu.h"
#include "pin_mux.h"
#include "clockMan1.h"
#include "dmaController1.h"
#include "osif1.h"
#include "canCom1.h"

  volatile int exit_code = 0;


/* User includes (#include below this line is not maintained by Processor Expert) */
#define MB (0UL)
#define MSG_ID (0UL)

/*!


  \brief The main function for the project.
  \details The startup initialization sequence is the following:
 * - startup asm routine
 * - main()
*/


int main(void)
{
  /* Write your local variable definition here */
 flexcan_data_info_t dataInfo =
 {
 .data_length = 1U,
 .msg_id_type = FLEXCAN_MSG_ID_STD,
 .enable_brs = false,
 .fd_enable = false,
 .fd_padding = 0U
 };
 uint8_t toggleLED = 0x55;

 

  /*** Processor Expert internal initialization. DON'T REMOVE THIS CODE!!! ***/
  #ifdef PEX_RTOS_INIT
    PEX_RTOS_INIT();                   /* Initialization of the selected RTOS. Macro is defined by the RTOS component. */
  #endif
  /*** End of Processor Expert internal initialization.                    ***/

  /* Write your code here */
  /* For example: for(;;) { } */


CLOCK_SYS_Init(g_clockManConfigsArr, CLOCK_MANAGER_CONFIG_CNT, g_clockManCallbacksArr, CLOCK_MANAGER_CALLBACK_CNT);
CLOCK_SYS_UpdateConfiguration(0U, CLOCK_MANAGER_POLICY_FORCIBLE);

 

PINS_DRV_Init(NUM_OF_CONFIGURED_PINS, g_pin_mux_InitConfigArr);


FLEXCAN_DRV_Init(INST_CANCOM1, &canCom1_State, &canCom1_InitConfig0);
FLEXCAN_DRV_ConfigTxMb(INST_CANCOM1,MB, &dataInfo, MSG_ID);

 

for(;;)
{
    if(GPIO_HAL_ReadPins(PTD)>>0==1)
    {
     GPIO_HAL_ClearPins(PTC,1<<0);
     FLEXCAN_DRV_Send(INST_CANCOM1,MB, &dataInfo, MSG_ID, &toggleLED);  
    }
    else
    {
     GPIO_HAL_SetPins(PTC,1<<0);
    }
}

Original Attachment has been moved to: CAN_FD_1.zip

标签 (1)
0 项奖励
回复
1 回复

1,501 次查看
martin_kovar
NXP Employee
NXP Employee

Hello,

this question is very similar to your second question posted in this thread:

https://community.nxp.com/message/885252 

I sent question to SDK application team and I am waiting for answer. I will write you the answer to the second thread as soon as I have any information for you.

Regards,

Martin

0 项奖励
回复