Hi all, I have a question about S32K312 MPU Background Region:
For example, setting permissions for a certain address: region1:permissions are readable and executable in privileged mode and readable and executable in user mode; So the permissions within the address area of region 1 are readable and executable in privileged mode and readable and executable in user mode; The access permissions for address segments other than region 1 are:
1.If the Background Region is enabled, the permissions for other address segments are: readable , writable, and executable under privileged mode, and not readable , writable, and executable under user mode?
2. If the Background Region is not enabled, what are the permissions for other address segments: not readable, not writable, and not executable under privileged mode and user mode?
Best regards.
Solved! Go to Solution.
Hi @sunyy,
As per the description, default memory map has read/write in both privileged and not-privileged modes. The background region has read/write in privileged mode only.
Please contact ARM support if you need more datails.
Regrads,
Daniel
Hello @sunyy,
This is specified in the documentation I linked here.
The background region has the same memory access attributes as the default memory map, but is accessible from privileged software only.
Please contact ARM support if you need more details.
Regards,
Daniel
Hi @sunyy,
As per the description, default memory map has read/write in both privileged and not-privileged modes. The background region has read/write in privileged mode only.
Please contact ARM support if you need more datails.
Regrads,
Daniel