the password to uncensor

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

the password to uncensor

975件の閲覧回数
hjhjhj
Contributor IV

Hi,

    Now there is something wrong in my MPC5643L, and its Package is 144 pins.It seems that it has been censored.Can anybody heip me solve it?

    11.png

Thank you!

HJ

0 件の賞賛
返信
1 返信

814件の閲覧回数
stanish
NXP Employee
NXP Employee

Hi 

This message might not always mean the device is really secured. Sometimes it could be misinterpreted with connection issue. The only way to censor the device is to intentionally write to "Shadow Flash" area which requires a specific algorithm to be used.

Could you possibly check if you have SBC chip on board enabled?  It may reset the MCU before the debug session is established.

Could you try to load a test project into RAM instead of flash?

Stan

0 件の賞賛
返信