Where can I download the Standalone installer for S32K14x SDK EAR 0.8.4?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where can I download the Standalone installer for S32K14x SDK EAR 0.8.4?

1,021 Views
sumityadav
Contributor II

This is referred to in the SDK documentation page 19 in the SDK documentation.

Thanks!

1 Reply

825 Views
martin_kovar
NXP Employee
NXP Employee

Hello,

unfortunately, there is not standalone installer for this version of SDK. SDK EAR 0.8.4 was delivered directly with S32 Design Studio version 2.0. It seems this is some general notice in documentation, which is not correct for this version.

But I strongly do not recommend you use this version of SDK. If you want to work with SDK, please use the newest version EAR 0.8.6, but remember, this is still Early Release Version, which is in development phase and which does not have to be compatible with newer version or with RTM (Release To Manufacturing) version.

Regards,

Martin