What does "Program finished with error #-1073741819" mean?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

What does "Program finished with error #-1073741819" mean?

跳至解决方案
2,331 次查看
9610wk
Contributor I

When I use S32 Flash Tool and click "Upload target and algorithm to hardware...", the software shows an error with "Program finished with error #-1073741819". What does this mean and how can I solve this problem?

图片1.png

0 项奖励
回复
1 解答
2,181 次查看
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @9610wk , 

 

Please can you check uninstalling the current version of USB/ FTD drivers and installing newer one. 

 

You can find the latest FTDI driver at : https://ftdichip.com/drivers/d2xx-drivers/

 

Please let me know if it works or not. 

 

Thank you. Kind regards. 

 

-Mehul Patel

在原帖中查看解决方案

0 项奖励
回复
5 回复数
2,307 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @9610wk 

The following community post discusses this topic, so please take a look at them. 

 

B.R.

VaneB

0 项奖励
回复
2,231 次查看
9610wk
Contributor I

Hi, VaneB

    Thanks for your reply. I read the listed post but the issue still exists.

    I checked the user guide for the evaluation board, installed 'SW32G2_RTD_4.4_2.0.0_HF04_DS_updatesite_D2107' and 'SW32G2_S32DS_3.4.1_D2104'. I also checked the listed conditions in the post and the check results are as follows.

    1.The USB connection between the PC and the target was attempted on one USB port.

    2.The target is set to ‘serial boot mode’ .

    3.The USB cable and other device are good as they can work on my colleague's PC.

    4.There were no other serial connections active on the same COM port at the same time the S32 Flash Tool was in use.

    5.The COM port be entered using UPPERCASE letters.

    6.None of the DIP switches are damaged.

    7.The error was reported after I clicked 'Upload target and algorithm to hardware...'

    Are there any other possible reasons for this issue? Thanks a lot

0 项奖励
回复
2,182 次查看
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @9610wk , 

 

Please can you check uninstalling the current version of USB/ FTD drivers and installing newer one. 

 

You can find the latest FTDI driver at : https://ftdichip.com/drivers/d2xx-drivers/

 

Please let me know if it works or not. 

 

Thank you. Kind regards. 

 

-Mehul Patel

0 项奖励
回复
2,126 次查看
9610wk
Contributor I

Hi, Mehul Patel

I'm sorry I only saw your reply today.

I solved the problem by uninstalling S32DS v3.4 and installing S32DS v3.5.

Thanks for your reply.

0 项奖励
回复
2,095 次查看
Mehul_Patel_NXP
NXP Employee
NXP Employee

Hi, @9610wk , 

 

Great that you were able to solve the issue. 

 

Yes, older version of tool might have issue because of old packages/ drivers and solved the With newer Deign Studio. 

 

Thank you for your reply. Happy coding. 

- Mehul 

0 项奖励
回复