WARNING - Selected .PCP file has been modified in S32R294 EVB Board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

WARNING - Selected .PCP file has been modified in S32R294 EVB Board

Jump to solution
1,753 Views
HyunungPark
Contributor III

I try to download new firmware into S32R294 EVB Board.

But it happens "WARNING - Selected .PCP file has been modified" like the below log.

Could you please let me know what I should do to resolve this issue? 

Device IDCODE is $000001F8
Device ID revision is $00000000
Initializing Ram Block 0x40000000-0x40007FFF.
S32R294 Device detected.
Target has been RESET and is active.
CMD>CM C:\NXP\S32DS_Power_v2.1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_2.0.4.202103012147\lin\gdi\P&E\macronix_mx25u25645g_quadspi_s32r294.pcp

Initializing.

Device IDCODE is $000001F8
Device ID revision is $00000000
Initializing Ram Block 0x40000000-0x40007FFF.
S32R294 Device detected.
Initialized.

;version 1.03, 07/15/2019, Copyright P&E Microcomputer Systems, www.pemicro.com

;device Macronix, MX25U25645G, 1x32x8192k, desc=QuadSPI_S32R294

;begin_cs device=$20000000, length=$02000000, ram=$40000000

Loading programming algorithm ...

WARNING - Selected .PCP file has been modified. CRC16 = $3BB5
Done.
Programming sequency is : erase, blank check, program, and verify {default}
CMD>VC
Command is inactive for this .PCP file.
VC is not implemented, falling back to VM

BRs.

Hyunung Park

0 Kudos
Reply
1 Solution
1,698 Views
HyunungPark
Contributor III

Hi,

This issue is resolved.

Thanks.

View solution in original post

0 Kudos
Reply
2 Replies
1,702 Views
juan_see
Contributor III

Hi Hyunung Park, 

You can safely ignore that message. It does not hinder functionality. 

0 Kudos
Reply
1,699 Views
HyunungPark
Contributor III

Hi,

This issue is resolved.

Thanks.

0 Kudos
Reply