S32DS for Power - Cant start debug session on Win10 laptop

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32DS for Power - Cant start debug session on Win10 laptop

1,386件の閲覧回数
uditsalunke
Contributor III

S32DS for PowerPc (DevKit 5748g) - Installation on Win10 wont allow debugging over OpenSDA.

GDB debug session could not be started. The same version works fine on Win 7. 

While installing S32DS, installer through error that Jungo Connectivity Driver is not "digitally signed" and so windows 10 won't allow   debugging session to start. 

Any one facing this issue? 

0 件の賞賛
返信
2 返答(返信)

1,165件の閲覧回数
uditsalunke
Contributor III

I updated P&E drivers as per P&E tech support and it fixed the issue.

Udit

0 件の賞賛
返信

1,165件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

I tried start debug session on Win10 64bit Pro version (fresh install) - and everything is working properly. Did you allow access for PE micro debug server in firewall settings? 

Jiri

0 件の賞賛
返信