Hello,
I'm sorry for all of the difficulties.
Please try these commands:
1) java -Djava.library.path=D:\NXP\CLL_FNP.11.18.0.2\lib\ -jar com.nxp.s32ds.rcp.license.core.jar install -prod S32DS-IDE-ARM_2.2
2) java -Djava.library.path=D:\NXP\CLL_FNP.11.18.0.2\lib\ -jar com.nxp.s32ds.rcp.license.core.jar activate -actid 8AF8-2BC1-1919-26A8
3) java -Djava.library.path=D:\NXP\CLL_FNP.11.18.0.2\lib\ -jar com.nxp.s32ds.rcp.license.core.jar list
It seems we need to get this installed BEFORE you try the command:
D:/NXP/S32DS_ARM_V2.2/jre/bin/java -Djava.library.path=D:/NXP/Activation/cll/i86 -jar D:/NXP/Activation/license.jar" activateUI
However, if you use the second command above, and it works, then you won't need to perform the activateUI command.
Best Regards,
Mike
Hello @LatromPu,
There are 2 possible causes for this issue.
1) It could be that your firewall is blocking access to the activation server. If this is the case, it can be resolved by either activating from another network or device outside of your current network or by using the offline activation method.
2) It could be the issue described under error 2 in the troubleshooting article:
Troubleshooting: Activation fails with error messa... - NXP Community
Best Regards,
Mike
Hi @mikedoidge ,
I try to use 5G net to activation the s32ds, and download the CLL_FNP file. it show can't find dependent libraries, whether should i download other libraries?
Hi @LatromPu,
Did you try the offline activation method? it is described in the installation guide and here:
HOWTO: Activate S32 Design Studio
Could you please execute the command: java -version
It could be the wrong version of java is used. S32DS install includes the correct version, but since your install is not completing, it may not be available when you use the CLL_FNP activation method.
If you try to install to C:\ instead of D:\, is the issue the same?
Best Regards,
Mike
Hello,
There is another possible solution to this issue:
Use the attached archive.
Enter the following command replacing the paths as noted. It should be possible to execute from CMD window located at any path. Make sure to use the ‘/’ instead of ‘\’ and if you have any paths with spaces, then enclose the full path with “.
C:/NXP/S32DS.3.5/jre/bin/java -Djava.library.path="{path to where you extracted the activation.zip}/Activation/cll/x64" -jar "{path to where you extracted the activation.zip}/Activation/license.jar" activateUI
Please try this and let us know if the issue is solved.
Best Regards,
Mike
Hi,
My apologies, I copied the instructions from my notes. I see you used the x64 version of the CLL libraries, since your machine has 32-bit, you should use the 'i86' CLL libraries for the 32-bit version. Please try the steps again.
Best Regards,
Mike
Hello,
I'm sorry for all of the difficulties.
Please try these commands:
1) java -Djava.library.path=D:\NXP\CLL_FNP.11.18.0.2\lib\ -jar com.nxp.s32ds.rcp.license.core.jar install -prod S32DS-IDE-ARM_2.2
2) java -Djava.library.path=D:\NXP\CLL_FNP.11.18.0.2\lib\ -jar com.nxp.s32ds.rcp.license.core.jar activate -actid 8AF8-2BC1-1919-26A8
3) java -Djava.library.path=D:\NXP\CLL_FNP.11.18.0.2\lib\ -jar com.nxp.s32ds.rcp.license.core.jar list
It seems we need to get this installed BEFORE you try the command:
D:/NXP/S32DS_ARM_V2.2/jre/bin/java -Djava.library.path=D:/NXP/Activation/cll/i86 -jar D:/NXP/Activation/license.jar" activateUI
However, if you use the second command above, and it works, then you won't need to perform the activateUI command.
Best Regards,
Mike
Hi @LatromPu
For S32 Design Studio for Arm it's supported host operating systems (OS):
B.R.
VaneB