S32DS3.4 add the FlexCan RTD Driver in S32K312 project issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS3.4 add the FlexCan RTD Driver in S32K312 project issue

Jump to solution
1,332 Views
Bert2023
Contributor III

Hi Sir:

IThe chip we use is S32K312,add the FlexCan RTD Driver ,it did not  build success. More inform as below:

Create Project:file--->new----->S32DS Application Project-------->select "S32K312"------->PlatformSDK_S32K3_2022_07_S32K312_M   2.0.1------> add the "FlexCan" driver in the "Component"


Tool:S3DS3.4

RTD:PlatformSDK_S32K3_2022_07   version:2.0.1

the error information as attachment picture error.jpg。

Thanks!

0 Kudos
Reply
1 Solution
1,281 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @Bert2023 

Just to be sure, did you click the "Update Code" button at Config Tools after adding FlexCan?

 

B.R.

VaneB

View solution in original post

0 Kudos
Reply
2 Replies
1,282 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @Bert2023 

Just to be sure, did you click the "Update Code" button at Config Tools after adding FlexCan?

 

B.R.

VaneB

0 Kudos
Reply
1,258 Views
Bert2023
Contributor III

Hi,VanB:

click the "Update Code" button at Config Tools after adding FlexCan, this way can solve  this issue.

Thanks!

0 Kudos
Reply