Is there a problem with the Offline activation of S32DS? I have created the request.xml using the activation code provided by Software & Support : Licensing. When using the activation.xml file returned by Software & Support I get an Invalid Offline Response. The installer then roll back the installation.
Original Attachment has been moved to: S32_Design_Studio_for_ARM_v1.2_Install_07_21_2016_07_39_18_2.log.zip
I tried many times, but the installation failed. The installer awalys rolls back the installation.Is the installation environment is not correct? Need to install online or offline?
What can Ido ?
hello, i hava same problem with you, can you give me solution?
ThankYou!
There could be several reasons why you cannot install S32DS:
Fail to install S32DS for Power Architecture v1.2
S32 Design Studio Offline activation issue hot fix
Stan
Hello,
Thanks for your report!
Could you possibly attach the installation log?
"c:\nxp\S32DS_ARM_v1.3\_S32 Design Studio for ARM v1.3_installation\Logs\S32_Design_Studio_for_ARM_v1.3_Install_*.log"
Our team is now investigating this issue.
Seem to be the same problem as reported here:
https://community.nxp.com/thread/439892
Stan
Dear Team:
My customer headaches for the same problem. We have tried different activation codes but none of them works.
Could you help to check this issue?
Thanks and Regards,
Wang
Hi I see you have
And have already activated this in machine 5615DB52D7BF1 , I have reset your keys, you should be able to use this key on your activation, please contact me if you have any issues.
Hello all,
I am also not able to make an offline activation. I tried also with suggested activation code 37D6-B186-B306-B6AA but it is also not working: "Invalid offline response, ResponseType"
I tried also logged in as the built in user Administrator -> the same result.
Best regards,
Hello Han,
Apologize about inconveniences.
Have you had another instance of S32DS v1.1 installed and activated already?
Could you possibly try to activate it once again (online/offline).
If it does not work with your original activation ID could you give a try with the "workaround" one we published:
37D6-B186-B306-B6AA
Thanks!
Stan
Hi Stan,
Just now I tried to install S32 with my original activation ID but is came the same issue discripted in my early reply today(both online and offline).
So there maybe some restrict about this SW in our company's network, according to your experence, is this reasonable or there are some other problems?
Hi Stan,
Thanks for your kindly reply.
Last weekend I have tried on my PC at home and there's no installation issue with my original activation ID.
But I also tried 37D6-B186-B306-B6AA last week and there is another issue shown below if I choose activate online, offline method was still the same. All of this happened on the laptop on my workplace . I will try again today. Thanks!
online
offline
Hi Paul,
First of all we apologize about the inconveniences. We are currently experiencing some activation issues on a small fragment of activation codes.
According to our records, you finally activated the tool. Am I right?
If not can you possibly try to activate (online/offline) using the testing activation code below:
37D6-B186-B306-B6AA
Please let us know if it works
Thanks!
Stan
Hi Stan,
I also encountered this issue when I install the S32 Design Studio for ARM v1.2, I tried to activate the SW online or offline but both failed. Is there something wrong with my activation code? Thanks a lot!
Hello Stan,
Unfortunately I get the same Invalid Offline Response. Should I try running the activation online? I can take my laptop home with me tonight and run the installation on my home network to see if the online activation works.
Best regards,
Paul Zak
Hello Paul,
Have you been able to activate the S32DS based on Allen suggestion?
Does the testing activation code work on your side (Online method)?
Thanks for your feedback!
Stan
Hello Stan,
I have tried the online activation from home and the installation fails. I get the following dialog.
The error log shows the same failure as with the offline activation.
Install Uninstaller: S32 Design Studio for ARM v1.2(Install All Uninstaller Components)
Status: ERROR
Additional Notes: ERROR - Error writing LaunchAnywhere components (Access Denied)
Is there anything else you can suggest?
Best regards,
Paul Zak
Hello Tomas,
I have tried both of the request files provided using offline activation. The first one (request1.xml) fails with invalid offline response. The second one (Request2.xml) fails with "Error processing offline response".
Best regards,
Paul
Paul
Thank you for the response Zak , I will review them an reply asap.
Have you been able to resolve the installation issue that I am having? I see this thread is assumed answered but I still can not install S32DS.