Hi, @chuanlin ,
The error seems to indicate that S32DS3.5 is not able to find the gdb client. (Or probably missing command gdb launch in debug configuration.) The gdb client is specified in the debug configuration. Please check that the default setting is as below:
Please can you check and get back.
Thank you, Best regards,
- Mehul Patel
Hi, @Mehul_Patel_NXP
Such issue was met under Windows-11.
Can you help to confirm whether S32DS_3.5 could run under Win11 correctly?
Thanks
Oliver
Hi, @OliverTian ,
Sorry for the late reply.
Is the issue still persist?
Please can you provide more information to understand the issue.
Thank you. Best regards.
- Mehul
Hi, Mehul
I re-installed WIN10 to overcome such issue. No more test under WIN11 after met such issue.
Hope WIN11 is supported and listed on the introduction of S32DS_3.5 in www.nxp.com
Regards
Oliver
Hi, Mehul
I re-install WIN10 to overcome such issue. No more test on WIN11 after met such issue.
Hope WIN11 could be supported and listed on S32DS_3.5's introduction in www.nxp.com
Regards
Oliver