Dear NXP Community,
I have a similar but different problem as described here:
https://community.nxp.com/t5/NXP-Model-Based-Design-Tools/Device-is-not-detected-or-may-be-censored-...
- When trying to enter debug mode the Warning: "Warning: Device is not detected or may be censored. ..."
- I have the Rev. B Board and the 3V3 LED does not light. (Different to the problem above)
- Pressing the reset button does not trigger reset (neither the red nor the yellow LED light up)
Any ideas what I could do or check?
With kind regards
Claudius
J11 jumper is set to 2-3 (USB Powered 5V Supply, through OpenSDA Interface).
We have other boards here that work seamlessly. It's only the one board that seems to have some issues.
Side note: As we don't have a 12 V External Supply, when setting the jumper to 1-2 neither of the status LEDs (5V / 3V3) lights.
It looks that probably 3.3V V reg is broken (or something shorts 3.3V power path) . You can try to figure out. Here is schematic for devkit board: https://www.nxp.com/webapp/sps/download/preDownload.jsp?render=true
Jiri
@jiri_kral thanks for the fast replies and the reference to the schematic devkit.
The question remains. What can I do about it. As far as I see it, I cannot resolve either of the two issues (irrespective of what is actually the problem).
Is there anything else that I could do?
Hi,
first of all you need to check 3.3V power regulator/power path. If there is no 3.3V power for MCU, MCU can't run (and you can't debug it). There is no other option what else you can do.
BR
Jiri