Hi,
I cant install S32 Design Studio for ARM v2.0 on Windows 7.
There is a error entry in the installation log:
Install Uninstaller: S32 Design Studio for ARM v2.0(Install All Uninstaller Components)
Status: ERROR
Additional Notes: ERROR - Error writing LaunchAnywhere components (Access Denied)
I have tired to run the installation as a normal user as well as administrator (Right click -> Run as Administrator). But installation still fails.
Is there a solution for this?
Thanks
Sean Lin
Hi 天雄 林,
Please check the windows service "Server" status.
Installanywhere relies on the service.
Make sure the "Server" service is enabled and running.
Then retry the installation.
Hello,
i'm having the same issue with "S32DS_Power_Win32_v2017.R1_b171019", is there a solution ?
Regards,
Hi
I tried a lot of method, but couldn't solve the problem, and finally installed win10
Hi Sean,
I'd strongly recommend you to install the latest version of S32DS (there is also the update 1 available).
It includes some new features and bug fixes.
S32 Design Studio for ARM 2018.R1 (Windows/Linux) released!
S32 Design Studio for ARM 2018.R1 - Update 1 available
Also please try to remove broken installation folder, close all other programs, and re-run the downloaded installer without admin rights.
Please attach the log from this version if the problem persists.
Thanks,
Stan
I have the same issue with installing S32DS_ARM_v2.2,the active license license couldn‘t popup and it rolled back,is there a solution?
Hi Stan,
First thanks for your help.
I tried to install the latest version of S32DS but the problem persists...
And I paste the log, wait for your help.
log:
Installation: Unsuccessful.
19 Successes
0 Warnings
1 NonFatalErrors
1 FatalErrors
Action Notes:
None
Install Log Detail:
Check Disk Space: C:\NXP\S32DS__v2018.R1
Status: SUCCESSFUL
Additional Notes: NOTE - Required Disk Space: 6,419,380,807; Free Disk Space: 14,434,590,720
Check Disk Space: C:\NXP\S32DS_ARM_v2018.R1
Status: SUCCESSFUL
Additional Notes: NOTE - Required Disk Space: 6,419,380,807; Free Disk Space: 14,434,590,720
Check Disk Space: D:\NXP\S32DS_ARM_v2018.R1
Status: SUCCESSFUL
Additional Notes: NOTE - Required Disk Space: 6,419,380,807; Free Disk Space: 10,664,316,928
Install Directory: D:\NXP\S32DS_ARM_v2018.R1\jre
Status: SUCCESSFUL
Install JRE: D:\NXP\S32DS_ARM_v2018.R1\jre
Status: SUCCESSFUL
Install Directory: C:\Users\geniusxiong\AppData\Local\Temp\669755.tmp\
Status: SUCCESSFUL
Additional Notes: NOTE - Directory already existed
Execute Command: NET SESSION
Status: SUCCESSFUL
Execute Command: ping 1.1.1.1 -n 1 -w 10000
Status: SUCCESSFUL
Install Uninstaller: S32 Design Studio for ARM Version 2018.R1(Install All Uninstaller Components)
Status: SUCCESSFUL
Install Directory: D:\NXP\S32DS_ARM_v2018.R1\_S32 Design Studio for ARM Version 2018.R1_installation\resource\
Status: SUCCESSFUL
Install File: D:\NXP\S32DS_ARM_v2018.R1\_S32 Design Studio for ARM Version 2018.R1_installation\resource\iawin32.dll
Status: SUCCESSFUL
Install File: D:\NXP\S32DS_ARM_v2018.R1\_S32 Design Studio for ARM Version 2018.R1_installation\resource\win64_32_x64.exe
Status: SUCCESSFUL
Install File: D:\NXP\S32DS_ARM_v2018.R1\_S32 Design Studio for ARM Version 2018.R1_installation\resource\remove.exe
Status: SUCCESSFUL
Install File: D:\NXP\S32DS_ARM_v2018.R1\_S32 Design Studio for ARM Version 2018.R1_installation\resource\invoker.exe
Status: SUCCESSFUL
Install Uninstaller: S32 Design Studio for ARM Version 2018.R1(Install All Uninstaller Components)
Status: ERROR
Additional Notes: ERROR - Error writing LaunchAnywhere components (Access Denied)
Uninstall Folder: D:\NXP\S32DS_ARM_v2018.R1\jre
Status: SUCCESSFUL
Uninstall Folder: D:\NXP\S32DS_ARM_v2018.R1
Status: SUCCESSFUL
Remove Registry Entry: 5 HKEY_LOCAL_MACHINE\SOFTWARE\Microsoft\Windows\CurrentVersion\Uninstall\null
Status: SUCCESSFUL
Error occurred while installing the following Action, hence rolling back the installation....!
Action Name: Trigger Rollback Action
Action Description: Trigger Rollback Action
Error Details as below:
This action rolls back the Installation.
====================STDERR ENTRIES==================
__________________________________________________________________________
InstallAnywhere 2014 SP1
Version: 16.5
__________________________________________________________________________
Wed Apr 04 08:57:42 CST 2018
Free Memory: 10547 kB
Total Memory: 15872 kB
No Arguments
Thanks,
Sean Lin
Sean,
have you been able to enter your activation code (see below) during the installation?
Hi Stan,
No, I did not go into this process.
Thanks,
Sean Lin
Hi,
Did you get the solution?