What is the difference between Flexray_43_LLCE_Ip.h and Fr_43_LLCE.h?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What is the difference between Flexray_43_LLCE_Ip.h and Fr_43_LLCE.h?

ソリューションへジャンプ
1,483件の閲覧回数
dantaki
Contributor II

I am trying to use Flexray on the S32G3.

I see that LLCE 1.0.7 drivers contain both Flexray_43_LLCE_Ip.h and Fr_43_LLCE.h. They both seem to include/implement similar functions. Flexray_43_LLCE_Ip.h seems to match more closely to what is in the S32G3 reference manual (S32G3RM).

The FlexRay examples use the Fr_43_LLCE.h functions.

 

Thanks for the help!

David

 

ラベル(1)
0 件の賞賛
返信
1 解決策
1,459件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

In general, the "_Ip" denotes that the file is not AUTOSAR compliant. Reviewing the content of both files, we see that the one that does not have the "_Ip" word on it shows the following note under the header:

DanielAguirre_0-1714576496073.png

While the one that has the "_Ip" does not show it.

Please, let us know.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,460件の閲覧回数
Daniel-Aguirre
NXP TechSupport
NXP TechSupport

Hi,

In general, the "_Ip" denotes that the file is not AUTOSAR compliant. Reviewing the content of both files, we see that the one that does not have the "_Ip" word on it shows the following note under the header:

DanielAguirre_0-1714576496073.png

While the one that has the "_Ip" does not show it.

Please, let us know.

0 件の賞賛
返信