Hi,
I cant install S32 Design Studio for ARM v2.0 on Windows 7.
There is a error entry in the installation log:
Install Uninstaller: S32 Design Studio for ARM v2.0(Install All Uninstaller Components)
Status: ERROR
Additional Notes: ERROR - Error writing LaunchAnywhere components (Access Denied)
I have tired to run the installation as a normal user as well as administrator (Right click -> Run as Administrator). But installation still fails.
Is there a solution for this?
Thanks
Sean Lin
Hello,
i'm having the same issue with "S32DS_Power_Win32_v2017.R1_b171019", is there a solution ?
Regards,
Hi
I tried a lot of method, but couldn't solve the problem, and finally installed win10
Hi Sean,
I'd strongly recommend you to install the latest version of S32DS (there is also the update 1 available).
It includes some new features and bug fixes.
S32 Design Studio for ARM 2018.R1 (Windows/Linux) released!
S32 Design Studio for ARM 2018.R1 - Update 1 available
Also please try to remove broken installation folder, close all other programs, and re-run the downloaded installer without admin rights.
Please attach the log from this version if the problem persists.
Thanks,
Stan
Hi Stan,
First thanks for your help.
I tried to install the latest version of S32DS but the problem persists...
And I paste the log, wait for your help.
log:
Installation: Unsuccessful.
19 Successes
0 Warnings
1 NonFatalErrors
1 FatalErrors
Action Notes:
None
Install Log Detail:
Check Disk Space: C:\NXP\S32DS__v2018.R1
Status: SUCCESSFUL
Additional Notes: NOTE - Required Disk Space: 6,419,380,807; Free Disk Space: 14,434,590,720
Check Disk Space: C:\NXP\S32DS_ARM_v2018.R1
Status: SUCCESSFUL
Additional Notes: NOTE - Required Disk Space: 6,419,380,807; Free Disk Space: 14,434,590,720
Check Disk Space: D:\NXP\S32DS_ARM_v2018.R1
Status: SUCCESSFUL
Additional Notes: NOTE - Required Disk Space: 6,419,380,807; Free Disk Space: 10,664,316,928
Install Directory: D:\NXP\S32DS_ARM_v2018.R1\jre
Status: SUCCESSFUL
Install JRE: D:\NXP\S32DS_ARM_v2018.R1\jre
Status: SUCCESSFUL
Install Directory: C:\Users\geniusxiong\AppData\Local\Temp\669755.tmp\
Status: SUCCESSFUL
Additional Notes: NOTE - Directory already existed
Execute Command: NET SESSION
Status: SUCCESSFUL
Execute Command: ping 1.1.1.1 -n 1 -w 10000
Status: SUCCESSFUL
Install Uninstaller: S32 Design Studio for ARM Version 2018.R1(Install All Uninstaller Components)
Status: SUCCESSFUL
Install Directory: D:\NXP\S32DS_ARM_v2018.R1\_S32 Design Studio for ARM Version 2018.R1_installation\resource\
Status: SUCCESSFUL
Install File: D:\NXP\S32DS_ARM_v2018.R1\_S32 Design Studio for ARM Version 2018.R1_installation\resource\iawin32.dll
Status: SUCCESSFUL
Install File: D:\NXP\S32DS_ARM_v2018.R1\_S32 Design Studio for ARM Version 2018.R1_installation\resource\win64_32_x64.exe
Status: SUCCESSFUL
Install File: D:\NXP\S32DS_ARM_v2018.R1\_S32 Design Studio for ARM Version 2018.R1_installation\resource\remove.exe
Status: SUCCESSFUL
Install File: D:\NXP\S32DS_ARM_v2018.R1\_S32 Design Studio for ARM Version 2018.R1_installation\resource\invoker.exe
Status: SUCCESSFUL
Install Uninstaller: S32 Design Studio for ARM Version 2018.R1(Install All Uninstaller Components)
Status: ERROR
Additional Notes: ERROR - Error writing LaunchAnywhere components (Access Denied)
Uninstall Folder: D:\NXP\S32DS_ARM_v2018.R1\jre
Status: SUCCESSFUL
Uninstall Folder: D:\NXP\S32DS_ARM_v2018.R1
Status: SUCCESSFUL
Remove Registry Entry: 5 HKEY_LOCAL_MACHINE\SOFTWARE\Microsoft\Windows\CurrentVersion\Uninstall\null
Status: SUCCESSFUL
Error occurred while installing the following Action, hence rolling back the installation....!
Action Name: Trigger Rollback Action
Action Description: Trigger Rollback Action
Error Details as below:
This action rolls back the Installation.
====================STDERR ENTRIES==================
__________________________________________________________________________
InstallAnywhere 2014 SP1
Version: 16.5
__________________________________________________________________________
Wed Apr 04 08:57:42 CST 2018
Free Memory: 10547 kB
Total Memory: 15872 kB
No Arguments
Thanks,
Sean Lin
Hi Stan,
No, I did not go into this process.
Thanks,
Sean Lin