Flash Multiple S32K144 Boards At Once?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Flash Multiple S32K144 Boards At Once?

1,430 次查看
mahmoudsherrah
Contributor III

Hello all,

1- I have multiple S32K144EVB boards connected to my PC and I wanted to flash the same SW project on all boards at the same time, either in parallel or one after the other automatically. Is it possible to achieve this?

2- Also if I need to flash different SW's to different boards, is there a way to automate this process with one button click?

P.S. I am using the standard PEMicro over OpenSDA to flash/debug.

Thanks.

0 项奖励
回复
4 回复数

1,292 次查看
mahmoudsherrah
Contributor III

Any ideas?

0 项奖励
回复

1,292 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

the OpenSDA is not designed for multiple flashing. You can flash two boards - just by connecting JTAG between two boards. The "master" board is connected to PC via OpenSDA. 

Jiri

0 项奖励
回复

1,292 次查看
mahmoudsherrah
Contributor III

Hello Jiri,

So flashing the master board would automatically flash the other one? Do you have an idea if this works for more than 2 boards?

Thanks

0 项奖励
回复

1,292 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

I already tested flashing two boards simultaneous. Further experiments/testing with OpenSDA and more boards is up to you.

Jiri 

0 项奖励
回复