Hello all,
1- I have multiple S32K144EVB boards connected to my PC and I wanted to flash the same SW project on all boards at the same time, either in parallel or one after the other automatically. Is it possible to achieve this?
2- Also if I need to flash different SW's to different boards, is there a way to automate this process with one button click?
P.S. I am using the standard PEMicro over OpenSDA to flash/debug.
Thanks.
Hello Jiri,
So flashing the master board would automatically flash the other one? Do you have an idea if this works for more than 2 boards?
Thanks