Hello!
I'm using the S32K3X8 Evaluation board.
Though I'm trying to change the clock division, it is failed because of error "MCU is not supported".
How can I solve this problem?
解決済! 解決策の投稿を見る。
It was caused by DRM in company.
it was resolved after decrypting the file 'S32V2xx.dsn.
Thank you.
Hello.
Thank you for answer. Unfortunately, I installed S32DS v3.5 and RTD for S32K358...
After posting this, I found the same issue with this. It was related with the DRM in laptop.
So, I need to check this point at first, then I'll get back.
Hi
Which version of S32K3 RTD did you install for S32DS v3.5? Please install RTD that supports S32K358. What I installed is S32K3_M27X Real-Time Drivers Version 3.0.0 P07. I can change the clock division in the Clocks tool of S32CT.
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
It was caused by DRM in company.
it was resolved after decrypting the file 'S32V2xx.dsn.
Thank you.