I am having the same issue as is described in another question, which has never been answered.
See "DEVKIT-MPC5748G c++ GDB server fails"
When using C++ classes with virtual methods, and the project gets compiled with Wind River Diab compiler, then the S32 Studion debugger crashes when loading the debug symbols.
Wind River Diab for PPC V5.9.4.7
S32 Design Studio for Power Architecture Version 1.2
GDB is powerpc-eabivle-gdb.exe version 7.8.2
Any new information on this issue?
Norbert Unterberg
Could you please attach some example ?
In previous thread topic starter's project was just invalid because of wrong linker script default.dld from Diab system root. While correct one for target HW should be resided in Project tree.