So, this is a similar issue as I have seen before which appeared to be down to a poorly soldered crystal. However, this board does not use an external crystal and the clock has been set to use FIRC.
I have configured all my clocks, peripherals and pins and then initialise them in a function.
//
// Setup the clocks.
//
CLOCK_SYS_Init(g_clockManConfigsArr, CLOCK_MANAGER_CONFIG_CNT, g_clockManCallbacksArr, CLOCK_MANAGER_CALLBACK_CNT);
CLOCK_SYS_UpdateConfiguration(0U, CLOCK_MANAGER_POLICY_AGREEMENT);
//
// Setup the I/O pins.
//
PINS_DRV_Init(NUM_OF_CONFIGURED_PINS0, g_pin_mux_InitConfigArr0);
//
// Setup the UART.
//
LPUART_DRV_Init(lpUartInstance, lpUartState, lpUartInitConfig);
LPUART_DRV_InstallRxCallback(lpUartInstance, rxCallback, NULL);
As soon as the code calls the PINS_DRV_Init, the processor crashes with a bus fault.
NUM_OF_CONFIGURED_PINS0 holds 8 and g_pin_mux_InitConfigArr0 looks like:
/* clang-format off */
/*
* TEXT BELOW IS USED AS SETTING FOR TOOLS *************************************
BOARD_InitPins:
- options: {callFromInitBoot: 'true', coreID: core0}
- pin_list:
- {pin_num: '38', peripheral: ADC0, signal: 'se, 0', pin_signal: PTA0}
- {pin_num: '40', peripheral: CAN1, signal: 'rxd, rxd', pin_signal: PTC6}
- {pin_num: '39', peripheral: CAN1, signal: 'txd, txd', pin_signal: PTC7}
- {pin_num: '41', peripheral: PORTA, signal: 'port, 13', pin_signal: PTA13, direction: OUTPUT}
- {pin_num: '17', peripheral: LPUART0, signal: rxd, pin_signal: PTC2}
- {pin_num: '16', peripheral: LPUART0, signal: txd, pin_signal: PTC3, direction: OUTPUT}
- {pin_num: '42', peripheral: PORTA, signal: 'port, 12', pin_signal: PTA12, direction: OUTPUT}
- {pin_num: '35', peripheral: PORTA, signal: 'port, 3', pin_signal: PTA3, direction: OUTPUT}
* BE CAREFUL MODIFYING THIS COMMENT - IT IS YAML SETTINGS FOR TOOLS ***********
*/
/* clang-format on */
/* Generate array of configured pin structures */
pin_settings_config_t g_pin_mux_InitConfigArr0[NUM_OF_CONFIGURED_PINS0] = {
{
.base = PORTA,
.pinPortIdx = 0U,
.pullConfig = PORT_INTERNAL_PULL_NOT_ENABLED,
.driveSelect = PORT_LOW_DRIVE_STRENGTH,
.passiveFilter = false,
.mux = PORT_PIN_DISABLED,
.pinLock = false,
.intConfig = PORT_DMA_INT_DISABLED,
.clearIntFlag = false,
.gpioBase = NULL,
.digitalFilter = false,
},
{
.base = PORTA,
.pinPortIdx = 12U,
.pullConfig = PORT_INTERNAL_PULL_NOT_ENABLED,
.driveSelect = PORT_LOW_DRIVE_STRENGTH,
.passiveFilter = false,
.mux = PORT_MUX_AS_GPIO,
.pinLock = false,
.intConfig = PORT_DMA_INT_DISABLED,
.clearIntFlag = false,
.gpioBase = PTA,
.direction = GPIO_OUTPUT_DIRECTION,
.digitalFilter = false,
.initValue = 0U,
},
{
.base = PORTA,
.pinPortIdx = 13U,
.pullConfig = PORT_INTERNAL_PULL_NOT_ENABLED,
.driveSelect = PORT_LOW_DRIVE_STRENGTH,
.passiveFilter = false,
.mux = PORT_MUX_AS_GPIO,
.pinLock = false,
.intConfig = PORT_DMA_INT_DISABLED,
.clearIntFlag = false,
.gpioBase = PTA,
.direction = GPIO_OUTPUT_DIRECTION,
.digitalFilter = false,
.initValue = 0U,
},
{
.base = PORTA,
.pinPortIdx = 3U,
.pullConfig = PORT_INTERNAL_PULL_NOT_ENABLED,
.driveSelect = PORT_LOW_DRIVE_STRENGTH,
.passiveFilter = false,
.mux = PORT_MUX_AS_GPIO,
.pinLock = false,
.intConfig = PORT_DMA_INT_DISABLED,
.clearIntFlag = false,
.gpioBase = PTA,
.direction = GPIO_OUTPUT_DIRECTION,
.digitalFilter = false,
.initValue = 0U,
},
{
.base = PORTC,
.pinPortIdx = 2U,
.pullConfig = PORT_INTERNAL_PULL_NOT_ENABLED,
.driveSelect = PORT_LOW_DRIVE_STRENGTH,
.passiveFilter = false,
.mux = PORT_MUX_ALT4,
.pinLock = false,
.intConfig = PORT_DMA_INT_DISABLED,
.clearIntFlag = false,
.gpioBase = NULL,
.digitalFilter = false,
},
{
.base = PORTC,
.pinPortIdx = 3U,
.pullConfig = PORT_INTERNAL_PULL_NOT_ENABLED,
.driveSelect = PORT_LOW_DRIVE_STRENGTH,
.passiveFilter = false,
.mux = PORT_MUX_ALT4,
.pinLock = false,
.intConfig = PORT_DMA_INT_DISABLED,
.clearIntFlag = false,
.gpioBase = NULL,
.digitalFilter = false,
},
{
.base = PORTC,
.pinPortIdx = 6U,
.pullConfig = PORT_INTERNAL_PULL_NOT_ENABLED,
.driveSelect = PORT_LOW_DRIVE_STRENGTH,
.passiveFilter = false,
.mux = PORT_MUX_ALT3,
.pinLock = false,
.intConfig = PORT_DMA_INT_DISABLED,
.clearIntFlag = false,
.gpioBase = NULL,
.digitalFilter = false,
},
{
.base = PORTC,
.pinPortIdx = 7U,
.pullConfig = PORT_INTERNAL_PULL_NOT_ENABLED,
.driveSelect = PORT_LOW_DRIVE_STRENGTH,
.passiveFilter = false,
.mux = PORT_MUX_ALT3,
.pinLock = false,
.intConfig = PORT_DMA_INT_DISABLED,
.clearIntFlag = false,
.gpioBase = NULL,
.digitalFilter = false,
},
};
If I step through the code with the debugger, it gets to:
for (i = 0U; i < pinCount; i++)
{
PINS_Init(&config[i]);
}
And on the first iteration of the above loop it crashes in here:
void PINS_Init(const pin_settings_config_t * config)
{
DEV_ASSERT(config->base != NULL);
DEV_ASSERT((PORT_MUX_AS_GPIO != config->mux) || (config->gpioBase != NULL));
DEV_ASSERT(config->pinPortIdx < PORT_PCR_COUNT);
uint32_t regValue = config->base->PCR[config->pinPortIdx];
uint32_t directions;
uint32_t digitalFilters;
port_mux_t muxing;
On the line
uint32_t regValue = config->base->PCR[config->pinPortIdx];
config->base holds 0x40049000 which I think is correct for port A and pinPortIdx holds 0.
Can anyone please help ?
Andy
已解决! 转到解答。
Hi
I try to disable crystal and SPLL of lpuart_s32k144w and select FIRC as clock source of LPUART. It will not enter fault.
Hi Andy,
It seems that the clock gate of PORTA is not enabled, so accessing the register of PORTA will cause fault.
Please call CLOCK_DRV_Init(&clockMan1_InitConfig0); instead of call CLOCK_SYS_Init(g_clockManConfigsArr, CLOCK_MANAGER_CONFIG_CNT, g_clockManCallbacksArr, CLOCK_MANAGER_CALLBACK_CNT);
CLOCK_SYS_UpdateConfiguration(0U, CLOCK_MANAGER_POLICY_FORCIBLE);
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Robin, thank you for your help.
Unfortunately, it now crashes while setting up the clock.
The stack trace looks like:
I get a "Possible BusFault location: 0x690B3A11" with the call to:
CLOCK_SYS_UpdateConfiguration(0U, CLOCK_MANAGER_POLICY_FORCIBLE);
Interestingly, in another project I have, I use CLOCK_SYS_Init and it works fine.
I actually love the way S32DS allows you to configure the peripherals and I/O and generate all the code for you however, it would be nice if it generated a file which did all this initialisation for us.
Andy
Okay, I was too quick to say it is fixed
I added a simple line to my main function and rebuilt and it is crashing setting up the oscillators again.
The line I added was:
LPUART_DRV_SendDataBlocking(lpUartInstance, (uint8_t *)oneSecondMsg, strlen(oneSecondMsg), TIMEOUT);
But it does not even get there as it fails right at the start of my code when I initialise the clock and peripherals. This is really, really frustrating.
Interestingly, sometimes when I single step, it gets through CLOCK_SYS_UpdateConfiguration(0U, CLOCK_MANAGER_POLICY_FORCIBLE) fine but then crashes as per the original way when PINS_DRV_Init(NUM_OF_CONFIGURED_PINS0, g_pin_mux_InitConfigArr0) is called !
Andy
Okay, so I have come back to the FS32K144 processor again and created a new project and I am again seeing a crash when initializing the I/O ports.
I have ensured that the SPLL and crystal clock paths are disabled and ensured the UARTS use the FIRC clock.
I have tried initializing the clock with:
CLOCK_SYS_Init( g_clockManConfigsArr, CLOCK_MANAGER_CONFIG_CNT, g_clockManCallbacksArr, CLOCK_MANAGER_CALLBACK_CNT );
CLOCK_SYS_UpdateConfiguration( 0U, CLOCK_MANAGER_POLICY_AGREEMENT );
and with:
CLOCK_DRV_Init( &clockMan1_InitConfig0 );
but the code is still crashing in:
PINS_DRV_Init( NUM_OF_CONFIGURED_PINS0, g_pin_mux_InitConfigArr0 );
with a Possible BusFault location: 0x40049000.
If I comment out the above pin initialization code and go on to initialize the UART with:
LPUART_DRV_Init( lpUSBUartInstance, lpUSBUartState, lpUSBUartInitConfig );
I get: An imprecise (asynchronous) data access error has occurred.
My clock configuration is:
I could really use some help getting to the bottom of this as I am on a tight deadline to get a project shipped.
Best Regards
Andy
https://community.nxp.com/t5/S32-SDK/SDK-problem-in-S32-Design-Studio-for-ARM-2-2/m-p/986190 Here you can find some information between CLOCK_DRV_Init and CLOCK_SYS_Init.
What's the version of S32K1xx SDK are you using? Please refer to the CLOCK_DRV_Init usage in hello_world_s32k144 of S32K1xx SDK RTM v4.0.3 Example Projects.
@Robin_Shen I am using SDK version 4.0.3.
I compared my configuration with a previous project that was working and noticed that I had set a flash clock divider of 4 to set the flash clock to 12MHz - in this current project is was a divisor of 2 (24MHz). Now that I have dropped the flash clock to 12MHz, it seems to be working.
Does this make sense? Is 24MHz too high for the flash memory?
Andy