Dear S32DS users,
S32 Design Studio for Power v1.1 Update 1 has been released.
The Offline update package could be downloaded here:
https://www.nxp.com/webapp/Download?colCode=S32DS_PA_v1.1_UP1&appType=license&location=null&Parent_n...
For online installation please select predefined NXP repository "Help" -> "lnstall New Software..." dialog:
${p2.metadata.repo.name} - http://www.nxp.com/lgfiles/updates/Eclipse/S32DS_POWER_1_1/com.freescale.s32power.updatesite
The list of changes:
- new compiler build 1.1.3 – see details in compiler release notes (attached)
- MS Visual C++ 2010 Redistributable x86 included for SPT tools for Windows 10
- Updated SPT tools:
- ENGR00381373 - Error build after Generate SPT
- Fixed ADD, SUB, CMP when destination register is different from src1
- ENGR00380758 64 bits operands are not supported for spt2 on windows
- Updated Examples
- New SPT1 example for MPC5775K
- o SingleElf_MPC5748G launch files updated with GDB command "set architecture powerpc:vle"
- Graph Tools
- ENGR00380255 [SPT] default graph should be created with standard includes
- Bug fixes:
- ENGR00375995 MPC5746C Embsys register definitons are missing SPI register set
- ENGR00379744 SPT assembler shall have initialized 'Include paths (-I) options after MPC577xK or S32R274 project creation
- ENGR00380796 Linker files section .spt should be corrected for SPT1/SPT2