When installing S32 Design Studio using the offline activation method (Offline activation on S32 ) the installer may pop up an error dialog: " Error: "Invalid offline response, ResponseType"." This typically occurs on the computers that have no previous installation of S32 Design Studio.
S32DS for ARM v1.1, v1.2, v1.3
S32DS for Power v1.1
S32DS for Vision v1.0
Newer versions should include the fix already.
Option A) Easiest solution is to use online method instead of offline. But in some cases it may not be possible (LAN restrictions, computer is not connected to the Internet or there is some other network obstacle etc.)
Option B) Apply the hot fix attached. See the instructions below how to proceed for Windows and Linux (Ubuntu) users
chmod 777 configure.sh
![S32DS_invalid_offline_linux1.png S32DS_invalid_offline_linux1.png](https://community.nxp.com/t5/image/serverpage/image-id/19777i0A443ADEC9AE3658/image-size/large?v=1.0&px=999)
sudo ./configure.sh install
![S32DS_invalid_offline_linux2.png S32DS_invalid_offline_linux2.png](https://community.nxp.com/t5/image/serverpage/image-id/19817i87813DC4A5A4E7CB/image-size/large?v=1.0&px=999)
sudo ./configure.sh reset
sudo ./configure.sh activate
Now you should be able to install S32 Design Studio on your computer.
Special thanks to denisrobert and zhongzhengliu for your help with fix testing and to all of you who reported this nasty issue. Thank you!!!
Stan
Hello Stan
I've tried this method,but it didn't work. It seems that the license can not be detected,and I still need to enter an activation code, but I got "Activation ID is already used on this station", could you help me?
Best regards,
Michael Von
Finally I solved this problem!
The ID I used before is unavailable,I ran licfix with ID:C699-XXXX-XXXX-E800 , after this process ,the installtion succeeded.
This is not working for me, tried both in Windows 10 and Ubuntu Linux. I get the same error as before for both online and offline activation. Tried with several activation codes given to me by NXP-staff.
this way is very very good , perfect solve my solution,thanks author!
Here I have a problem,
S32 Design Studio V1.2 starts failed after Offline activation installation, although there is information says the installation is successful. After the installation, I double click the icon to start the S32DS V1.2 IDE on my 64bit computer, which runs on a windows 7 OS, then it appears the information"An error has occurred.See the log file D:\software\s32_power_win32_v1.2\eclipse\configuration\1587541348989.log.", when I install it on a x86 computer, it starts normally after my double click the icon.
here are the contents of log files:
1. request.xml
<?xml version="1.0" encoding="UTF-8" ?><Request xmlns="http://www.macrovision.com/fnp/2004/11/activation"><RequestHeader><VersionNumber>3</VersionNumber><RequestType>ACTIVATION</RequestType></RequestHeader><RequestData><EntitlementData>
<EntitlementId>F5C1-454F-0B3F-D638</EntitlementId>
<ActivationReason>0</ActivationReason>
<ProductId>Not Applicable</ProductId><PublisherId>10295808</PublisherId>
</EntitlementData><OriginData><ClientVersion>11.13.0</ClientVersion><ConfigData><IsServer>0</IsServer><TrustedHostInformation><TrustedId>3</TrustedId><Revision>1</Revision><RevisionType>SRV</RevisionType><MachineIdentifier>C10B71177DE41388FFF8D8F63272A257460555DE</MachineIdentifier><Status>OK</Status></TrustedHostInformation></ConfigData>
<Platform>
<PlatformTypeName>i86_n3</PlatformTypeName>
<OperatingSystem><Info>none</Info></OperatingSystem>
</Platform>
<UniqueMachineNumbers>
<UniqueMachineNumber><Type>1</Type><Value>DD27C1ECE3C53BD3AF0066FECCEDDE48B08EBBB8</Value></UniqueMachineNumber>
<UniqueMachineNumber><Type>2</Type><Value>8DA5DC9D43A2734F9CFB439C9AAF6E918F126C23</Value></UniqueMachineNumber>
</UniqueMachineNumbers>
<SequenceNumber>1</SequenceNumber></OriginData><PublisherDictionary>
<Entries>
<Entry>
<Key>flexFulfillmentVersion</Key>
<Value>1</Value>
</Entry>
</Entries>
</PublisherDictionary></RequestData><Hash>36D5F97454FB2C75A57499FC6A34B353E6F1553C</Hash><HashVersion>1</HashVersion></Request>
2. activation.xml
<?xml version="1.0" encoding="UTF-8" ?><Response xmlns="http://www.macrovision.com/fnp/2004/11/activation"><ResponseHeader><VersionNumber>2</VersionNumber><ResponseType>ACTIVATION</ResponseType><RequestSequenceNumber>1</RequestSequenceNumber><RequestHash>36D5F97454FB2C75A57499FC6A34B353E6F1553C</RequestHash></ResponseHeader><ResponseData><EntitlementData><EntitlementId>F5C1-454F-0B3F-D638</EntitlementId><ProductId>Not Applicable</ProductId></EntitlementData><TrustedHostInformation><TrustedId>3</TrustedId><Revision>1</Revision><RevisionType>SRV</RevisionType><MachineIdentifier>C10B71177DE41388FFF8D8F63272A257460555DE</MachineIdentifier><Status>OK</Status></TrustedHostInformation><FulfillmentRecord><FulfillmentRecordHeader><VersionNumber>1</VersionNumber></FulfillmentRecordHeader><FulfillmentRecordData><FulfillmentId>172921657</FulfillmentId><FulfillmentDictionary><Entries><Entry><Key>serverHostId</Key><Value>INTERNET=0.0.0.0</Value></Entry><Entry><Key>fulfillmentIdChain</Key><Value>172921657</Value></Entry><Entry><Key>servOrLocal</Key><Value>2</Value></Entry><Entry><Key>availAct</Key><Value>1</Value></Entry><Entry><Key>fulfillmentType</Key><Value>6</Value></Entry><Entry><Key>actServerChain</Key><Value>https://nxp.flexnetoperations.com/control/frse/ActivationService</Value></Entry><Entry><Key>features</Key><Value>INCREMENT Activated freescale 1.2 16-jun-2023 1 \
VENDOR_STRING=S32-DS-E200_v1.2|F5C1-454F-0B3F-D638|NO_TRIAL \
DUP_GROUP=UHDV ISSUER="Freescale Semiconductor" \
ISSUED=22-apr-2020 ck=129 SN="FSL - 30328777" TS_OK SIGN="0296 \
8025 ACEC 5534 B687 E3DE D973 B0A1 8D15 1B55 1777 7F25 3555 \
602C 396C 11F6 D87B DC00 5A6C 1218 7276 19E0 D2B2 C66F 5780 \
6286 CC44 D71D 387D 5216"
</Value></Entry><Entry><Key>expiry</Key><Value>16-Jun-2023</Value></Entry><Entry><Key>productId</Key><Value>S32-DS-E200_v1.2</Value></Entry><Entry><Key>entitlementId</Key><Value>F5C1-454F-0B3F-D638</Value></Entry></Entries></FulfillmentDictionary></FulfillmentRecordData></FulfillmentRecord></ResponseData><Signature>0FA674232B263BB9B97E4DD99150D291CF78673E5245FA5012A37E72F55E13CA62F1D7ADF8AAA524505FD31C6C11FEC770C64C9333F88A29EE090292</Signature><SignatureVersion>1</SignatureVersion></Response>
3. 1587541348989.log
!SESSION 2020-04-22 15:42:28.833 -----------------------------------------------
eclipse.buildId=4.4.2.M20150204-1700
java.version=1.8.0_51
java.vendor=Oracle Corporation
BootLoader constants: OS=win32, ARCH=x86, WS=win32, NL=zh_CN
Framework arguments: -product com.freescale.s32ds.e200.ide
Command-line arguments: -os win32 -ws win32 -arch x86 -product com.freescale.s32ds.e200.ide
.......
.......
!ENTRY org.eclipse.osgi 4 0 2020-04-22 15:42:38.661
!MESSAGE Application error
!STACK 1
java.lang.RuntimeException: Application "org.eclipse.ui.ide.workbench" could not be found in the registry. The applications available are: org.eclipse.ant.core.antRunner, org.eclipse.cdt.codan.core.application, org.eclipse.cdt.core.GeneratePDOM, org.eclipse.equinox.app.error, org.eclipse.equinox.p2.director, org.eclipse.equinox.p2.garbagecollector.application, org.eclipse.equinox.p2.publisher.InstallPublisher, org.eclipse.equinox.p2.publisher.EclipseGenerator, org.eclipse.equinox.p2.publisher.ProductPublisher, org.eclipse.equinox.p2.publisher.FeaturesAndBundlesPublisher, org.eclipse.equinox.p2.reconciler.application, org.eclipse.equinox.p2.repository.repo2runnable, org.eclipse.equinox.p2.repository.metadataverifier, org.eclipse.equinox.p2.artifact.repository.mirrorApplication, org.eclipse.equinox.p2.metadata.repository.mirrorApplication, org.eclipse.equinox.p2.updatesite.UpdateSitePublisher, org.eclipse.equinox.p2.publisher.UpdateSitePublisher, org.eclipse.equinox.p2.publisher.CategoryPublisher, org.eclipse.help.base.infocenterApplication, org.eclipse.help.base.helpApplication, org.eclipse.help.base.indexTool, org.eclipse.jdt.core.JavaCodeFormatter, org.eclipse.jdt.core.JavaIndexer.
at org.eclipse.equinox.internal.app.EclipseAppContainer.startDefaultApp(EclipseAppContainer.java:248)
at org.eclipse.equinox.internal.app.MainApplicationLauncher.run(MainApplicationLauncher.java:29)
at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.runApplication(EclipseAppLauncher.java:134)
at org.eclipse.core.runtime.internal.adaptor.EclipseAppLauncher.start(EclipseAppLauncher.java:104)
at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:380)
at org.eclipse.core.runtime.adaptor.EclipseStarter.run(EclipseStarter.java:235)
at sun.reflect.NativeMethodAccessorImpl.invoke0(Native Method)
at sun.reflect.NativeMethodAccessorImpl.invoke(Unknown Source)
at sun.reflect.DelegatingMethodAccessorImpl.invoke(Unknown Source)
at java.lang.reflect.Method.invoke(Unknown Source)
at org.eclipse.equinox.launcher.Main.invokeFramework(Main.java:648)
at org.eclipse.equinox.launcher.Main.basicRun(Main.java:603)
at org.eclipse.equinox.launcher.Main.run(Main.java:1465)
How to solve this problem under an Offline activation installation method?
Thank you.
yours Jakie.
Hi,
This problem does not seems to be related to the activation since the generated XML response is ok.
It rather seems like an eclipse is missing some plugins. Can you try to download the installer again and try to reinstall S32DS.
I'd suggest you to install the lateset greatest version:
https://community.nxp.com/docs/DOC-343864
Regards,
S.
Sorry to bother you.
I also encountered problems with the installation(S32DS_PA V2.1).
I also tried the relevant solutions in the community, but I couldn't solve the problem.
Thanks in advance for your help.
Hello I'm trying to dlownload for a previous version v2.0 and v2.2 is already installed on my local pc. so when I'm trying to get the activation xml file it is giving me this error message again and again. Can anyone please help me on this?