cannot understand SYS instruction for S12XE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

cannot understand SYS instruction for S12XE

1,571 Views
Xbot
Contributor II
hi,
 
i'm having a hard time understanding the purpose of the SYS instruction. this is supposed to an MPU call. is this an interrupt call where you can enter supervisor state? how about when i want to set the descriptors for XGATE code execution, how do do it?
 
there is also interrupt vectors for access errors ?
Labels (1)
0 Kudos
Reply
1 Reply

790 Views
Steve
NXP Employee
NXP Employee
SYS is an additional "software interrupt" that does the same kind of thing as SWI. It was added because SWI is already heavily used in debugging environments. The intent of SYS is to provide a separate software interrupt for use by the system that will not cause confusion and difficulties for development tools.
All interrupts including SYS return you to supervisor state.
Read AN3242 for more information about the MPU and SYS and Supervisor and User State.
0 Kudos
Reply