Is it possible to have manual control of the SS pin while using SPI. I would like to interface with a 16 bit SPI devise (MC33810) where the SS signal is required but it must not return to idle between transmission of the two bytes. I have seen this devise used with the same microcontroller so there is presumably a way of doing it but i dont have access to the code.
Cheers