I test s12p128 ATD base on KIT33812ECUEVME Evaluation Board, the ATD always can't collect a value.
As for hardware, the partial pressure of VBAT collected by AN0, is measured at 3.6V.
First,I use PE to config ATD,but it can't collect a value.
Second,I refer to S12G128 demo code,Configured as a single measurement.
Teset with the same problem.
The S12P128 ATD need other peculiar setup ? BTY,Do you have a separate ATD routine for S12P128?Tks!
Hi,
I recommend you to look at the document AN2428 and AN3937 MC9S12P-Family Demonstration Lab Training, there can be found the S12P ADC Demo code with description.
AN3937:
https://www.nxp.com/files-static/microcontrollers/doc/app_note/AN3937.pdf
SW:
http://www.nxp.com/files/microcontrollers/doc/app_note/AN3937SW.zip
AN2428 – An Overview of the HCS12 ATD Module:
https://www.nxp.com/docs/en/application-note/AN2428.pdf
I believe it helps you.
Best regards,
Diana
Hi,
just small hit/idea:
If I remember correctly, one of KIT33812ECUEVME versions has incorrectly assembled diode (in the wrong direction) for measuring battery voltage (according to User Guide, it should be D2).
I reported it a few years ago, but I am not sure, whether already assembled boards were fixed or not.
Nothing dangerous, please just check diode orientation.
I hope it helps you.
Best Regards
Radek