Replace the MCU R5F10CMDxFB of Renesas in auto application

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Replace the MCU R5F10CMDxFB of Renesas in auto application

620 次查看
lukegu
Contributor I

Dear ,

        One of my customer wants to replace the MCU with the PN R5F10CMDxFB. The necessary peripherals as followings :

      Package :LQFP 80

      Interfaces :  LCD Drivers , more than  3ch  ADCs (10bit or above resolution ) , 1 ch CAN(2.0B) , more than 5 Timers , 1ch I2C, 1ch SPI, 2ch UART ;

      Power supply : 3.3 V--5V (5V will be better)

      Could you kindly help me to check this issue and give me some recommand MPN? Appreciated a lot !

标签 (1)
0 项奖励
回复
1 回复

516 次查看
RadekS
NXP Employee
NXP Employee

Hi Luke,

I would like to recommend S12ZVH family (ZVH, ZVHY, ZVHL, ZVFP):

http://www.nxp.com/products/automotive-products/microcontrollers-and-processors/16-bit-s12-magniv/s1...

This is highly integrated solution powered directly from 12V (you don’t need external power regulator), up to 40x4 LCD Segment driver, up to 4 Stepper Motor Controllers and potentially also with CAN or LIN physical layer.

Optionally there are also slightly older S12XHY or S12HY families:

http://www.nxp.com/products/automotive-products/microcontrollers-and-processors/16-bit-s12-s12x-mcus...

http://www.nxp.com/products/automotive-products/microcontrollers-and-processors/16-bit-s12-s12x-mcus...

Unfortunately, none of these MCUs are not available in LQFP 80 package. Only LQFP 64, 100, 112, 144 packages are available.

I hope it helps you.

Have a great day,
Radek

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复