Please help to configure CW 10.6 to flash application to MC9S12ZVA192 using IC5000 emulator

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Please help to configure CW 10.6 to flash application to MC9S12ZVA192 using IC5000 emulator

795 次查看
shijoabraham
Contributor II

I am using isystem's IC5000 for connecting micro controller suing CW 10.6. But, not sure about the configuration to be done. Please help

0 项奖励
回复
3 回复数

714 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

HI

I wonder IC5000 can't support S12Z device but IC3000 can. see

NXP - Partner Profile Information 

Click on "device" you will see which devices are supported by the tool.

pastedImage_2.png

to work with IC3000, the recommend IDE is winIDEA.

If using CodeWarrior, the supported programming/debug prob is P&E tool or Open source BDM.


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

714 次查看
shijoabraham
Contributor II

Hi,

Thank you very much for the valuable information.

IC3000 will work with CodeWarrior and IC5000 not. Is it?

0 项奖励
回复

714 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

No, both IC3000 and IC5000 can't work with CodeWarrior. They work with winIDEA.


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复